Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv Launches Energy-Efficient, Scalable UPS for Edge and Mid-sized Applications in EMEA

October 03, 2023

The compact Vertiv™ Liebert® APM2 uninterruptible power supply system is compatible with Li-ion and VRLA batteries

London, UK [October 3, 2023] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced the Vertiv™ Liebert® APM2, a new energy-efficient and scalable power solution to its uninterruptible power supply (UPS) systems portfolio. The Liebert® APM2 is compatible with lithium-ion (Li-ion) and VRLA batteries and features a compact design that can scale from 30kW to 600kW in a single unit. It offers significant energy savings compared to less efficient alternatives, and can also parallel with up to four matching units for additional capacity or redundancy. The Liebert APM2 is a CE certified UPS system available in 400V in Europe, the Middle East and Africa, Latin America, and Asia, including India and China. 

To satisfy the increasing power needs of edge computing applications, as well as the constrained space typical of these sites, Liebert APM2 delivers a greater power output in a smaller footprint than similar capacity solutions, with Liebert APM2 models requiring up to 45% less space than the predecessor UPS, Vertiv™ Liebert® APM. The Liebert APM2 can be installed in-row, in-room, against-the-wall, or back-to-back for further application flexibility. 

"Vertiv created the Liebert APM2 in response to the need for a compact and efficient product that delivers dependable power quality and availability to the network edge,” said Kyle Keeper, senior vice president of global AC power at Vertiv. “The UPS is Vertiv's cutting-edge solution for handling increasing power infrastructure needs without the need for a complete system overhaul.” 

The Liebert® APM2 operates with high energy efficiency in all modes, up to 97.5% in double-conversion mode; up to 98.8% efficiency when operating in Dynamic online mode, which draws power through the bypass line and uses the inverter for balanced output and as an active filter; and up to 99% when operating in ECO mode, which takes advantage of stable grid input conditions to leverage the bypass line. All modes are automated based on user preferences.  The intelligent paralleling feature of the Liebert APM2 facilitates load sharing among multiple power modules, even across multiple units. This enables balanced unit runtime and offers automatic failover for enhanced system availability. Intelligent paralleling has also been shown to contribute to energy efficiency

“Vertiv has introduced, in Liebert APM2 and other UPS systems, enhancements that improve operational efficiency and can contribute to a reduced data center PUE while also maintaining system availability,” said Giovanni Zanei, senior director AC power global offering & EMEA business leader at Vertiv. “In particular, the Dynamic Online feature, built on a robust global platform launched in 2018, enhances the already impressive UPS efficiency and has been adopted by energy- and availability-conscious customers, including many colocators.”

The modular architecture of the Liebert APM2 allows for easy front-side access to replaceable components and features hot-swappable building blocks that optimise the mean time to repair (MTTR) to less than 30 minutes. The Vertiv™ Life™ Services program is an available option to remotely monitor and diagnose equipment health, with reporting to track UPS performance. 

For more information on the Liebert APM2 and other UPS solutions from Vertiv, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centres, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise. 

CONTACT

Susanna Collins
T +44 (0)7872 558593
E susanna.collins@apodpr.o.uk

PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location