Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv Expands Power Portfolio with Enhanced Static Transfer Switch for Critical Applications in EMEA

May 22, 2025

Vertiv™ PowerSwitch 7000 enables high-availability power architectures for data centres, providing enhanced reliability through seamless power source transfers

London, UK [May 22, 2025] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure today announced the launch of the Vertiv™ PowerSwitch 7000, a next-generation static transfer switch that strengthens Vertiv's position as a complete power solutions provider. The system further expands the end-to-end portfolio of Vertiv solutions that enable the critical digital world to continuously accelerate and perform. Designed to support uninterrupted operations across vital sectors including data centres, financial services, and manufacturing technology, Vertiv PowerSwitch 7000 addresses the growing demand for power reliability in an increasingly digital world. Available now in Europe, Middle East and Africa markets, this solution supports continuity in power supply to help prevent costly disruptions.  

Vertiv PowerSwitch 7000 operates downstream from redundant uninterruptible power supply (UPS) systems in reserve bus and dual-bus power architectures for facilities that cannot tolerate power interruptions, including colocation and enterprise data centres. The system delivers seamless, automatic transfers between independent power sources, providing critical redundancy for both single-corded loads and additional protection for dual-corded equipment. An internally redundant architecture further eliminates potential single points of failure.

"Power protection and reliability are increasingly critical concerns for data centre operators, especially when planning for computing growth," said Greg Hoge, product management global director at Vertiv. "By combining reliable switching, operational flexibility, maintenance simplicity, and intelligent diagnostics, Vertiv PowerSwitch 7000 sets a high standard for operational excellence in power switching technology for even the most demanding data centre applications."

The upgraded system offers innovative serviceability features that include a compartmentalised design that separates high-voltage sections from maintenance areas, enhancing operator safety while improving overall serviceability. The front-access design allows maintenance without service interruption, reducing repair time while maintaining continuous power to critical loads. Flexible installation options, including top and bottom cable entry, make it ideal for both raised and non-raised floor environments. Modular SCRs (Silicon Controlled Rectifiers), hot-swappable fan assemblies, and tool-free air filters support quick servicing and consistent performance. 

The on-unit 9-inch colour touchscreen control panel provides advanced waveform capture capability, allowing the platform to function as a diagnostic tool, by capturing power measurements at a high sampling rate during transfer events to support comprehensive root cause analysis. This intelligent monitoring system provides facility managers with easy access to system data, helping them quickly identify and respond to power disturbances. Remote monitoring is available through Vertiv™Intellislot™ RDU120 communication card, which is UL2900-1 cybersecurity certified, delivering secure, remote access to system status and diagnostics.

Vertiv™ PowerSwitch 7000 integrates seamlessly with Vertiv's comprehensive portfolio of power management systems, including UPS systems and power distribution units, creating a complete power protection ecosystem. The solution is supported by Vertiv™ Global Services, a worldwide network of trained experts offering a comprehensive portfolio of project, lifecycle, and digital services to maximise reliability and minimise downtime.

For more information about the Vertiv PowerSwitch 7000 and Vertiv's power management solutions, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centres, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the

Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT

Susanna Collins
T +44 (0)7872 558593
E susanna.collins@apodpr.co.uk

PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location