Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv SmartAisle™ Receives TIER IV-Ready Award from Uptime Institute in Asia

August 07, 2018

Singapore [August 07, 2018] – Vertiv, formerly Emerson Network Power, today announced that its SmartAisle™ solution was granted a TIER IV-Ready Certification by the Uptime Institute in Asia, the first in the company's portfolio of IT and edge infrastructure solutions in the region to achieve this distinction. A TIER IV-Ready certification is the highest certification, signifying maximum reliability and efficiency of the solution.

The TIER IV-Ready certification was awarded to a specific model of the SmartAisle only available in Asia and was evaluated based on a number of factors, including design specification, site-specific information, network topology, as well as mechanical and electrical components.

The Uptime Institute found that the Vertiv SmartAisle supports a Fault Tolerant design, with redundant capacity and modularity. This enables the data center to potentially function within the requirements of a total design for TIER IV certifications, according to the Uptime Institute.

"We are thrilled that Vertiv has achieved Uptime Institute's TIER-Ready certification for their latest SmartAisle solution. Pre-fabricated and modular solutions that display the TIER-Ready logo are a customer's assurance that the design they are considering has been certified by Uptime Institute for its ability to deliver resilience across a wide range of operating conditions," said Christopher Brown, chief technology officer of Uptime Institute.

The latest SmartAisle series from Vertiv provides a simplified, rapid deployment data center design in a row-based system. Its fully integrated features include power, thermal management, infrastructure management and monitoring, as well as racks and containment, offering considerable savings for data center operators. The Vertiv SmartAisle solution is modular and scalable depending on capacity requirements, and is capable of supporting deployments for Internet of Things (IoT) applications and edge computing networks.

"We are proud to receive the TIER IV-Ready Certification from the Uptime Institute. This is a testament to our commitment and investment to continuously introduce new products and solutions that support the current and the future needs our customers ," said Chee Hoe Ling, vice president of product, solutions and marketing at Vertiv in Asia. "The Vertiv SmartAisle is a best-in-class, fully-integrated, customizable, easy to deploy and intelligent solution that is ready to support the fast deployment of critical applications at the core and edge of the network. Trust that we will strive to continuously innovate with new technologies and solutions that support our customers in this fast-evolving market landscape."

For further information, visit www.VertivCo.com/SmartAisle.

About Vertiv
Vertiv designs, builds and services critical infrastructure that enables vital applications for data centers, communication networks and commercial and industrial facilities. Formerly Emerson Network Power, Vertiv supports today's growing mobile and cloud computing markets with a portfolio of power, thermal and infrastructure management solutions including the Chloride®, Liebert®, NetSure™ and Trellis™ brands. For more information, visit VertivCo.com.

CONTACT
Katrina Tirante
T +6326203600 Ext 7666
E Katrina.Tirante@vertivco.com

Reinier Dungca
T +6326203600 Ext 7657
E Reinier.Dungca@vertivco.com

CTA
PARTNERS
Overview
Consultants Corner
PARTNERS
Overview
Consultants Corner

Language & Location